This website uses cookies and similar technologies in order to optimize its functionalities through the production of anonymous and statistical data. No correlation is made between such cookies and nominative information Legrand may hold.
Learn more
I refuse
I accept
Select a language
English (United Kingdom)
español (España)
Home
FAQ
Configuration
I need to replace F460, how can I do that?
Is it possible to calibrate the thermostats of MyHome installation?
Which measure of time is used for sunrise and sunset condition that I can use as trigger and condition for scenes?
How many F422A I can add to an installation with F460?
Which functions can be configured with the BT-F522, BT-F523 and BT-*4672N and the other flush mounted products?
Can I use F460 for MyHomeSuite SW?
How can I add one object in the system?
How can I identify one actuator of my installation if I cannot reach it?
Where I can set the thresholds of humidity logic in the F460?
How can I set the load control system?
Where I can set the fade-in and fade-out parameters of a Dali2 lamps?
Can MyHOME installation manage an energy meter?
Is it possible with F460 to export the SCS addresses configuration of the installation?
How can I configure the energy meter?
Does F460 request a dedicated power supply?
Can I manage Dali2 lamps with F460?
Which are the differences between F429D and F429G?
Can not find the answer to your questions ?
Our Customer Service is here to help you
Contact us